结果 "CPI"
Selected Options
Chatsworth Products (CPI) Extended limited warranties on CPI-Branded Electronic hardware products are available for two additional years beyond the expiration of the Original Warranty Period (3 years).
6 选项
Starting at 243.81 USD MSRP
Chatsworth Products (CPI) Extended limited warranties on CPI-Branded Non-Electronic hardware products are available for two additional years beyond the expiration of the Original Warranty Period (3 years).
6 选项
Starting at 102.41 USD MSRP
The PatchRack is a miniature two-post rack that can be attached to CPI Cable Runway to save rack-mount space by placing patch panels or interconnect equipment above the rack or cabinet.
16 选项
Starting at 197.86 USD MSRP
CPI's Raised Floor Grommets provide a reliable seal around cable bundles. The rectangular grommet features a dual-layer brush with an integrated EPDM membrane for a superior seal. The Round grommet option offers a cabling solution in limited spaces.
2 选项
Starting at 70.85 USD MSRP
The Adjustable Rail QuadraRack (ARQR) provides a sturdy, feature-rich solution for supporting rack-mount network, computer server and data storage equipment in data centers, computer equipment rooms and other IT facilities.
18 选项
Starting at 1344.14 USD MSRP
Bonding Jumpers provide common bonding from equipment rack or cabinet to the Telecommunications Equipment Bonding Conductor.
2 选项
Starting at 48.60 USD MSRP
CPI's patent-pending Tool-less Cross Member Radius Drop supports and guides cable loads as they enter and exit the runway, allowing cables to maintain proper bend radius.
27 选项
Starting at 40.82 USD MSRP
QuadraRack® 4-Post Frame provides the stability and strength of an enclosure in a open mounting system.
6 选项
Starting at 113.25 USD MSRP
The Standard Rack is a high quality, cost-effective storage solution for patch panels and network switches that use less floor space than a cabinet or a four-post rack. Built-in attachment point for a ground (earthing) connection.
15 选项
Starting at 262.67 USD MSRP
Provides double-sided 6” (150 mm) cable run between equipment racks.
12 选项
Starting at 711.15 USD MSRP
改善方式
改善方式
  • News and Events [63]
Selected Options
认可展示了CPI在定制的独特边缘解决方案方面的专长 加利福尼亚州阿古拉山(Agoura Hills),10月2019年1月1日-年度布线安装与维护(CI&M)创新者奖最近授予Chatsworth Products(CPI)两个金奖,以表彰该公司解决边缘网络独特挑战的前瞻性方法。   在应用程序和案例研究类别中,CPI因展示在线食品服务公司如何成功地将其网络扩展到制造环境而不放弃宝贵的建筑面积而获得认可,这要归功于一个定制 详细的CPI主导的项目 ,该项目包括与多个利益相关者的协作,多种配置选项和最终解决方案,包括带有双排气冷却单...
Chatsworth Products 获得气流创新的多项额外专利   所获多项专利展示了 CPI 对技术创新和优秀设计的不懈求索     加州阿古拉山,2018 年 1 月 5 日 — 气流管理和 Passive Cooling® 技术的创造者 Chatsworth Products (CPI) 宣布在其具有突破性和开创性的长长数据中心产品列表中又添数项全新专利。   在支持和保护关键网络设备方面提供行业领先的 IT 基础设施产品,CPI 已有 26 年以上的雄厚经验。CPI 提供的产品包括数据中心应用,如管道排气机柜、通道密...
迪拜,阿拉伯联合酋长国,2015 年 6 月 19 日 — 位于阿布扎比的 Regents Emirates Pearl Hotel 预计是世界上最豪华的酒店之一。在 IT 基础设施和设备全球制造商 Chatsworth Products (CPI) 的帮助下,此豪华空间拥有最先进的数据中心,能满足未来几年里的技术需求。 为了与酒店服务业的顶级酒店竞争,Regents Emirates Pearl Hotel 和 CPI、咨询与工程公司 Atlas Telecom 以及数据中心解决方案分销商 MultiNet Communications ...
提供极佳的设备支持,无论尺寸或型号如何 加利福尼亚西湖村,2014 年 4 月 22 日 – 使用来自 Chatsworth Products (CPI) 的全新重新设计的 N 系列 TeraFrame® Gen 3 机柜系统,支持并保护网络交换机,无论尺寸、型号或气流要求如何。N 系列 TeraFrame 让设备管理更进一步,支持在一台机柜中部署不同尺寸的设备,且无需额外配件组件,并可提供完全的气流隔离。 N 系列 TeraFrame 是一款用于高密度网络和存储交换机的网络机柜,可完全整合在任何数据中心封闭方案中,提供完整的...
免费、易用,并可随时随地提供快速结果! WESTLAKE VILLAGE, Calif.,2014 年 4 月 29 日 – Chatsworth Products (CPI) 自豪地推出其著名 Mini Catalog 的移动应用程序版,这是该公司的最新工具,用以帮助客户更快更便捷地开展业务。 CPI Mini Catalog 应用程序是一款免费工具,可下载至 Apple iPad 来帮助 IT 和电信专业人士轻松识别和选择产品。 CPI Mini Catalog 应用程序设计为一款独立应用程序,无需网络连接或登录信息...
挽救数据中心中浪费的电力和冷却能力 美国加利福尼亚西湖村 (WESTLAKE VILLAGE) – Chatsworth Products (CPI) 可向您展示如何通过通道封闭解决方案获得更快的投资回报率,并避免在新的数据中心上花费 500 万至 2500 万美元。 30% 至 50% 的数据中心在未来一年内将耗尽电量和冷却能力,且将使用比 IT 负载实际需要平均多四倍的冷却能力。使用气流封闭,您可以重新获得无法使用或丧失的能力,延长基础设施的使用寿命。事实上,新标准要求使用气流封闭作为提高任何数据效率的最低基准,如 ASHR...
Chatsworth Products 的全新可调节缆线桥架提供终极缆线桥架灵活性,定制 免工具配件提供显著的劳动力成本削减 加利福尼亚州西湖村,2016 年 1 月 15 日讯 — Chatsworth Products (CPI) 的全新可调节缆线桥架设计旨在打造高度灵活的点对点通道,以轻松支撑数据中心、电信机房和其他缆线进出通道的空间内的线缆和光纤。 CPI 的可调节缆线桥架包含可动式横向构件,有助于沿着桥架将组件和配件安装在不同位置,简化机架、机柜和缆线管理器之上的布线对齐过程。横向构件通过两个压纹螺丝固定在桥架纵桁...
冷通道封闭降低功耗并提升公司士气 加利福尼亚西湖村 (WESTLAKE VILLAGE),2013 年 12 月 4 日 – Chatsworth Products’ (CPI) 通道封闭解决方案通过使用应对数据中心结构和业务变化的独特方法,能够降低高达 50% 的用电量,从而实现资金节省和设施效率提升。 Hostirian,圣路易斯的一个主机托管提供商,最近将 4,500 平方英尺的办公空间转化成一个使用 CPI 的冷通道封闭 (CAC) 解决方案的数据中心,从而实现了用电量的显著下降。在重新设计前,Hostirian 曾...
在 ICT 和 Wi-Fi 基础设施的综合专业能力造福有志于拓展边缘产品的全球客户 加利福尼亚州阿古拉山市,2019 年 10 月 8 日 - Chatsworth Products (CPI)—作为信息和通信技术 (ICT) 基础设施、电源产品和工业机箱的全球制造商,已经完成对 Oberon Inc.,这家总部设在宾夕法尼亚州的无线接入点和天线安装解决方案提供商的收购。 两家公司的综合专业能力将造福所有有志于将其网络拓展到边缘和户外环境的客户,而经过优化的 CPI 产品组合现在包括更多样的室内和户外无线机箱和 Wi-Fi 安装解决方...
Chatsworth Products 迎来了提供优质解决方案,保护世界各地珍贵技术投资的第 25 个年头。 雇员所有制公司的创新历史为扩张、前沿解决方案提供动力 WESTLAKE VILLAGE, Calif.,2016 年 6 月 1 日 — 今年,Chatsworth Products 迎来了提供优质产品和解决方案,保护世界各地珍贵技术投资的第 25 个年头。CPI 是一家 100% 由雇员持有的公司,由一群致力于为快速发展的信息技术市场提供优质产品的个人成立。如今,CPI 在美国和全球均有工程设计、制造和销售办事处。...