结果 "CPI"
Selected Options
Chatsworth Products (CPI) Extended limited warranties on CPI-Branded Electronic hardware products are available for two additional years beyond the expiration of the Original Warranty Period (3 years).
6 选项
Starting at 243.81 USD MSRP
Chatsworth Products (CPI) Extended limited warranties on CPI-Branded Non-Electronic hardware products are available for two additional years beyond the expiration of the Original Warranty Period (3 years).
6 选项
Starting at 102.41 USD MSRP
The PatchRack is a miniature two-post rack that can be attached to CPI Cable Runway to save rack-mount space by placing patch panels or interconnect equipment above the rack or cabinet.
16 选项
Starting at 197.86 USD MSRP
CPI's Raised Floor Grommets provide a reliable seal around cable bundles. The rectangular grommet features a dual-layer brush with an integrated EPDM membrane for a superior seal. The Round grommet option offers a cabling solution in limited spaces.
2 选项
Starting at 70.85 USD MSRP
The Adjustable Rail QuadraRack (ARQR) provides a sturdy, feature-rich solution for supporting rack-mount network, computer server and data storage equipment in data centers, computer equipment rooms and other IT facilities.
18 选项
Starting at 1344.14 USD MSRP
Bonding Jumpers provide common bonding from equipment rack or cabinet to the Telecommunications Equipment Bonding Conductor.
2 选项
Starting at 48.60 USD MSRP
CPI's patent-pending Tool-less Cross Member Radius Drop supports and guides cable loads as they enter and exit the runway, allowing cables to maintain proper bend radius.
27 选项
Starting at 40.82 USD MSRP
QuadraRack® 4-Post Frame provides the stability and strength of an enclosure in a open mounting system.
6 选项
Starting at 113.25 USD MSRP
The Standard Rack is a high quality, cost-effective storage solution for patch panels and network switches that use less floor space than a cabinet or a four-post rack. Built-in attachment point for a ground (earthing) connection.
15 选项
Starting at 262.67 USD MSRP
Provides double-sided 6” (150 mm) cable run between equipment racks.
12 选项
Starting at 711.15 USD MSRP
改善方式
改善方式
Selected Options
全球分销合作伙伴和增值经销商 销售与全球经销商网络合作进行。 分销商通过随时向您提供全面的产品或产品来提供附加价值,并将告知您快速发展的通信技术领域的新发展和变化。 我们的专业经销商拥有强大的计划,以支持最终用户,承包商和安装人员,并随时准备支持您的需求。 某些领域可能还有其他经销商。 除了CPI的全球分销商网络外,CPI还与诚信企业合作,帮助您识别和采购适合您应用的产品和解决方案。 无论您需要完整的集成解决方案还是单个产品,请联系我们的增值经销商(VAR)合作伙伴。 寻找经销商或经销商。 承包商和系统集成商 CPI可以推...
以下软件支持CPI的各种电源和电子产品。 在下面选择适当的软件链接。 如需帮助, 请联系我们的技术支持团队 。   Software for eConnect Power Distribution Units eConnect ® Power Distribution Unit (PDU) File  Release Date Notes Firmware 5.3.1094 02-27-2024 Use only with individual eConnect units wi...
对于使用 AutoCAD 进行设计布局的客户,CPI 已建立常用 CPI 产品的 CAD 形状。 CPI CAD 形状拥有俯视图、正视图、侧视图和等距视图,且免费提供。 若要下载这些免费的 CAD 形状用于您的设计布局,点击下方链接。  将提示您保存 .zip 文件。 Zip 文件是需要 WinZip 软件来打开的压缩文件。 请访问 WinZip 网站 获取更多信息。 如果您在下方未找到特定产品,请拨打 +86 21 6880 0266 或发送电子邮件至 [email protected] 联系 CPI 技术支持。 ...
CPI 缆线填充表列出了所有 CPI 缆线管理和缆线布线路径产品的线缆填充推荐值和最大值。 利用此表能找到选用理线器或布线路径产品的线缆填充值。 该表列出了各理线器或布线路径产品的的可用面积,以便您计算其他类型的缆线。 填充表有两种格式,便携文件格式 (PDF) 和 Microsoft Excel 格式。                                      PDF 格式                  Excel 电子表格 * *这种电子表格使用简便, 您可以根据缆线规格快速估算缆线填充值。 理线器和布线路径产品...
CPI 还被多个重要国家组织授予多项奖项,对其业务理念和雇员所有制 结构表示肯定。   Awards: CPI has received the following awards (partial listing):  Year Awarded   Description 2021 CPI 的 ZetaFrame™ 机柜被选为布线安装和维护 (CI&M) 2021 年创新者奖的银级获奖者。 2021 Chatsworth Products 的一个部门 Oberon 因其 1018-00 ...
CPI 及其部门在创新和卓越方面引领行业,并已获得多项突破性产品设计专利。 专利:CPI 及其部门已获得以下专利:    Patent # Description CPI Products Covered by Patent 11,342,730 Ceiling Enclosure for Wireless Equipment Wi-Tile™ Locking Suspended Ceiling Zone Enclosure 1074 Series Wi-Tile™ Locking ...
CPI 致力于成为在其业务所有方面拥有最高品质的公司:优质产品、优质服务和最重要的优质员工。 优质产品 坚固耐用的结构 设计初衷是最大的功能性 进行工程设计时最优先考虑安全 许多产品经过 UL 认证 创新式设计 无数专利和奖励 安全包装,确保您的产品完好抵达 UL DQS Inc. 已认证 CPI 为 ISO 9001 认证公司 。 优质服务 对客户服务请求作出快速响应 来自专业销售人员的个性化解决方案 一对一提供布局配置和其他服务 自由 节省时间  设计工具 ,如 Visio Shapes、CAD 模块...