结果 "cable"
Selected Options
This sturdy play-out reel makes installing multi-conductor or coaxial cables a one-person job. The installer no longer needs to unwind the cable, lay it flat on the floor and have another installer assist by feeding the cable into the duct. 
1 选项
Starting at 970.17 USD MSRP
Electrically isolates Cable Runway sections, isolating grounding sections of runway or where strong EMI/RFI fields could generate eddy-currents, which could disturb down-line equipment.
2 选项
Starting at 35.68 USD MSRP
Allows the attachment of cable runway 12" (300 mm) directly above and either parallel or perpendicular to existing Cable Runway.
3 选项
Starting at 102.19 USD MSRP
Create a radius for L, T, or X-shaped intersections of Cable Runway.
8 选项
Starting at 142.07 USD MSRP
Permits the dropping of cables at any point between cross members of 9", 12" or 18"W (230 mm, 300 mm or 460 mm) Cable Runways. Combine with the recommended Cable Runway Radius Drop.
9 选项
Starting at 72.18 USD MSRP
Supports Cable Runway above a continuous row of CPI Racks or Cabinets of varying heights and provides additional space between the tops of the racks or cabinets and the cable runway, which can create smoother transition of cables.
16 选项
Starting at 61.39 USD MSRP
Pathway Dividers divide Cable Runway into multiple cable pathways in order to organize cables according to media type or destination.
8 选项
Starting at 39.47 USD MSRP
This bracket can be mounted at desired height and depth to position straps right where you need them reusable rivets allow Saf-T-Grips to be added or removed as required. Mounting hardware not included.
8 选项
Starting at 300.50 USD MSRP
The Cable Ring Kit is designed for the Evolution® Single-Sided Vertical Cable Manager. Creates a separate cable pathway for premise cables at the back of the Cable Manager. 
10 选项
Starting at 178.14 USD MSRP
Provides tie points for cable inside Velocity Vertical Cable Managers. Attaches to the mid panel with included hardware. Use in 6"W (152 mm) or wider vertical cable managers; one kit per side.
1 选项
Starting at 124.55 USD MSRP
改善方式
改善方式
Selected Options
Chatsworth Products 凭借 Motive 垂直理线器引领缆线管理新方式 免工具配件、独特的设计有助于实现无限制的调整,并最大限度使用内部空间 AGOURA HILLS, Calif.,2016 年 10 月 21 日 — Chatsworth Products (CPI) 以其在缆线管理方面的品质和专门技术而著称,最新发布的 Motive 垂直理线器也不例外,它是突破性设计以及一系列免工具配件的先驱者,在数据 中心行业中前所未有。 “Motive 垂直理线器完美地体现了 CPI 的独创性以及与客户的密切关系,能够...
机架级气流控制和集成电源管理先锋致力于拓展定制创新和增长 加利福尼亚州阿古拉山,2021 年 6 月 29 日今年是 Chatsworth Products (CPI) 公司 100% 员工持股 30 周年纪念,该公司致力于为全球动态复杂的信息和通信技术 (ICT) 行业提供创新基础设施解决方案。   CPI 成立于 1991 年,当时,90 名员工通过员工持股计划 (ESOP) 收购了 Harris 公司的 Dracon 部门,在互联网使用快速增长的时代,CPI 的存在推动公司开发了一系列影响深远的机架、跑道和缆线管理产品组合,改...
Chatsworth Products 发布下一代 EuroFrame™ 机柜 EuroFrame Gen 2 可为欧洲数据中心提供最新的经济可靠网络设备机柜 2017 年 10 月 20 日,英国白金汉郡 — Chatsworth Products (CPI) 宣布发表第二代 EF 系列 EuroFrame™ 机柜。EuroFrame Gen 2 是 CPI 推出的最新款经济性机柜,其设计在保持当今现代化数 据中心所需的高性能前提下,通过提供安装简单快捷的存储解决方案,最大限度缩减部署时间,减少部署所需资源。 EuroFrame...
加利福尼亚西湖村,2015 年 5 月 26 日 — 网络中立互连和数据中心公司 Cologix, Inc. 通过实施 Chatsworth Products (CPI) 的定制解决方案改善冷却低效问题,进而节省成本和能源。 随着八大市场之一北美市场的发展,Cologix 需要高品质且富有成本效益的解决方案来支撑和安放达拉斯 INFOMART 运营商酒店的结构化布线、电源产品和客户 IT 设备。 为解决冷却和气流低效问题,Cologix 评估了很多公司并选择了 CPI 的热通道封闭 (HAC) 解决方案,其包括 GF 系列 Globa...
Chatsworth Products 的全新第二代 GT 系列 GlobalFrame ® 机柜系统最大限度为数据中心应用节省资金 该机柜解决方案专为亚太市场打造,符合绿色要求。   上海,2016 年 5 月 17 日 - Chatsworth Products (CPI) 很高兴推出第二代 GT 系列 GlobalFrame ® 机柜系统,该计算机和网络设备储存解决方案专为帮助亚洲公司缩减整体能源成本并满足绿色标准而设计。 易于使用的第二代 GT 系列 GlobalFrame 机柜提供 14 种热门柜架尺寸,以满...
Chatsworth Products总结数据中心资产和机房面积的远程管理七步法     Chatsworth Products (CPI)发表的新白皮书显示,随着物联网(IoT)的不断发展,数据中心管理者可以将数据中心机柜作为一个完整生态系统的基础,降低资产和机房面积的远程管理难度。 这篇名为“数据中心机柜生态系统成功的关键要素”(The Key Elements of a Successful Data Center Cabinet Ecosystem)的白皮书认为,实现可用性、可靠性和能源效率的最有效和最直接的途径,是将基础架构、...
突破性设计提供最大限度的缆线调整和支持,不需要使用工具 加利福尼亚州 亚哥拉山, 2019 年 5 月 23 日 — 领先的数据中心、电信机房及周边基础设施产品制造商 Chatsworth Products (CPI) 宣布其 Motive ® 垂直理线器获得专利。  随着对更高数据速率、更高带宽和更高密度的需求与日俱增,CPI 认识到市场需要高度可配置的缆线管理解决方案,尤其是支持各种缆线介质的光缆,同时提供最佳的气流和缆线松弛度管理实践。 美国专利编号10,271,452 描述了一种垂直理线器,包括...
提供极佳的设备支持,无论尺寸或型号如何 加利福尼亚西湖村,2014 年 4 月 22 日 – 使用来自 Chatsworth Products (CPI) 的全新重新设计的 N 系列 TeraFrame® Gen 3 机柜系统,支持并保护网络交换机,无论尺寸、型号或气流要求如何。N 系列 TeraFrame 让设备管理更进一步,支持在一台机柜中部署不同尺寸的设备,且无需额外配件组件,并可提供完全的气流隔离。 N 系列 TeraFrame 是一款用于高密度网络和存储交换机的网络机柜,可完全整合在任何数据中心封闭方案中,提供完整的...
美国加利福尼亚西湖村 - 2012 年 7 月- Chatsworth Products, Inc. (CPI)是一家环球制造商,专门生产用于优化、存储和保护技术设备的产品与解决方案。该公司现已推出 OnTrac ®  定型金属网格式桥架,可使网络缆线的表面接触面积增加 400%。与许多标准型网格托架相比, OnTrac 定型桥架 使表面面积大幅增加,因此可在数据中心与网络设备机房中创建点对点布线路径,极为适合于支持高性能与高密度布线。  定型桥架将大多数金属网格桥架上使用的传统型圆形交叉线取代为独特的扁平交叉线,能够使与桥架接触的缆线所...
英国白金汉郡,2015 年 7 月 21 日 — 总部位于挪威的银行、保险和控股公司联盟 SpareBank 1 采用他们称之为“乐高 ® 策略”的手段,能够通过 Chatsworth Products (CPI) 灵活而创新的数据中心解决方案改善其数据中心基础设施并提高数据中心电力使用效率 (PUE)。 SpareBank 1 与 CPI 和数据中心解决方案供应商 Coromatic 合作,设计量身定制的一流数据中心,以满足需求。联盟想要匹配其需求且能够提供 200 kW 功率和冷却功能的解决方案,以保持运营的连续性。 为满足该独...