结果 "cable"
Selected Options
This sturdy play-out reel makes installing multi-conductor or coaxial cables a one-person job. The installer no longer needs to unwind the cable, lay it flat on the floor and have another installer assist by feeding the cable into the duct. 
1 选项
Starting at 970.17 USD MSRP
Electrically isolates Cable Runway sections, isolating grounding sections of runway or where strong EMI/RFI fields could generate eddy-currents, which could disturb down-line equipment.
2 选项
Starting at 35.68 USD MSRP
Allows the attachment of cable runway 12" (300 mm) directly above and either parallel or perpendicular to existing Cable Runway.
3 选项
Starting at 102.19 USD MSRP
Create a radius for L, T, or X-shaped intersections of Cable Runway.
8 选项
Starting at 142.07 USD MSRP
Permits the dropping of cables at any point between cross members of 9", 12" or 18"W (230 mm, 300 mm or 460 mm) Cable Runways. Combine with the recommended Cable Runway Radius Drop.
9 选项
Starting at 72.18 USD MSRP
Supports Cable Runway above a continuous row of CPI Racks or Cabinets of varying heights and provides additional space between the tops of the racks or cabinets and the cable runway, which can create smoother transition of cables.
16 选项
Starting at 61.39 USD MSRP
Pathway Dividers divide Cable Runway into multiple cable pathways in order to organize cables according to media type or destination.
8 选项
Starting at 39.47 USD MSRP
This bracket can be mounted at desired height and depth to position straps right where you need them reusable rivets allow Saf-T-Grips to be added or removed as required. Mounting hardware not included.
8 选项
Starting at 300.50 USD MSRP
The Cable Ring Kit is designed for the Evolution® Single-Sided Vertical Cable Manager. Creates a separate cable pathway for premise cables at the back of the Cable Manager. 
10 选项
Starting at 178.14 USD MSRP
Provides tie points for cable inside Velocity Vertical Cable Managers. Attaches to the mid panel with included hardware. Use in 6"W (152 mm) or wider vertical cable managers; one kit per side.
1 选项
Starting at 124.55 USD MSRP
改善方式
改善方式
Selected Options
CPI 缆线填充表列出了所有 CPI 缆线管理和缆线布线路径产品的线缆填充推荐值和最大值。 利用此表能找到选用理线器或布线路径产品的线缆填充值。 该表列出了各理线器或布线路径产品的的可用面积,以便您计算其他类型的缆线。 填充表有两种格式,便携文件格式 (PDF) 和 Microsoft Excel 格式。                                      PDF 格式                  Excel 电子表格 * *这种电子表格使用简便, 您可以根据缆线规格快速估算缆线填充值。 理线器和布线路径产品...
CPI 及其部门在创新和卓越方面引领行业,并已获得多项突破性产品设计专利。 专利:CPI 及其部门已获得以下专利:    Patent # Description CPI Products Covered by Patent 11,342,730 Ceiling Enclosure for Wireless Equipment Wi-Tile™ Locking Suspended Ceiling Zone Enclosure 1074 Series Wi-Tile™ Locking ...
对于使用 AutoCAD 进行设计布局的客户,CPI 已建立常用 CPI 产品的 CAD 形状。 CPI CAD 形状拥有俯视图、正视图、侧视图和等距视图,且免费提供。 若要下载这些免费的 CAD 形状用于您的设计布局,点击下方链接。  将提示您保存 .zip 文件。 Zip 文件是需要 WinZip 软件来打开的压缩文件。 请访问 WinZip 网站 获取更多信息。 如果您在下方未找到特定产品,请拨打 +86 21 6880 0266 或发送电子邮件至 [email protected] 联系 CPI 技术支持。 ...
对于使用Microsoft®Visio进行设备布局和网络图创建的客户,CPI与NetZoom合作创建了常见CPI产品的形状。 这些形状与Visio版本5/2000/2002/2003/2007兼容,并且免费提供。 若要下载这些免费 Visio 形状,请点击下方链接。 将提示您保存 .zip 文件。 Zip 文件是需要 WinZip 软件来打开的压缩文件。 请访问 WinZip 网站 获取更多信息。 要查看NetZoom的完整CPI NetZoom形状库或了解NetZoom,请 访问NetZoom网站 。   CPI 的 Vis...
CPI 还被多个重要国家组织授予多项奖项,对其业务理念和雇员所有制 结构表示肯定。   Awards: CPI has received the following awards (partial listing):  Year Awarded   Description 2021 CPI 的 ZetaFrame™ 机柜被选为布线安装和维护 (CI&M) 2021 年创新者奖的银级获奖者。 2021 Chatsworth Products 的一个部门 Oberon 因其 1018-00 ...
CPI 提供建筑师、工程师和其他设计专业人员,并拥有内容丰富的建筑信息建模 (BIM) 文件库,可用于起草和设计理想装置。 来自 Autodesk Seek® 的这些 Revit 型号制造用于达到 BICSI、Autodesk® Seek RMCSG 及其他组织的最新标准。 若要下载这些免费 BIM 文件,请点击下方链接。 将提示您保存 .zip 文件。 Zip 文件是需要 WinZip 软件来打开的压缩文件。 请访问  WinZip Website  获取更多信息。 通过下载以下文件,您同意我们的  许可协议。    机架系统 ...
以下软件支持CPI的各种电源和电子产品。 在下面选择适当的软件链接。 如需帮助, 请联系我们的技术支持团队 。   Software for eConnect Power Distribution Units eConnect ® Power Distribution Unit (PDU) File  Release Date Notes Firmware 5.3.1100 07-10-2024 Use only with individual eConnect units wit...