Results for "Jumper Trays"
Refine By
Selected Options
Designed to promote a gradual, controlled bend for both UTP and optical fiber cable. Slotted holes allow bend radius location to be user adjustable.
16 options
Starting at 190.46 USD MSRP
The Lower Jumper Tray, Double aids in compliance with ANSI/TIA/EIA-568B bend radius requirements. Designed to promote a gradual, controlled bend for both UTP and optical fiber cable.
8 options
Starting at 263.44 USD MSRP
The Lower Jumper Tray, Single aids in compliance with ANSI/TIA/EIA-568B bend radius requirements. Provides 1-1/2" (38 mm) bend radius for compliant installation of Category 5e/6/6a or fiber cable.
8 options
Starting at 219.55 USD MSRP
Optional transition plate creates a solid wireway between Racks With 3"D Channels.
4 options
Starting at 77.24 USD MSRP
The Rack Top-Mount Cable Trough mounts on top of CPI racks.
15 options
Starting at 74.68 USD MSRP
Refine By

    • Blogs [19]
Refine By
  • Blogs [19]
Selected Options
Chatsworth Products (CPI) offers a wide variety of horizontal cable managers that range from full-featured Evolution® Cable Managers (shown) to horizontal ring panels and jumper trays. These products can be used above and below patch panels and network switches to organize a...
In today’s high-density data centers, maintaining the integrity of fiber cables is crucial for uninterrupted data flow, operational efficiency, and long-term infrastructure health. With increasing demand for data-driven applications, including cloud computing, AI, and IoT, da...
If you’ve ever attended a standing-room-only, sold-out concert, you’ll have a good idea of where we’re coming from – first, imagine the amount of people – just a sea of faces as far as the eye can see. Everyone, pressed together, shoulder-to-shoulder, packed to the rafters. ...
When managing a data center, efficiency is often a top priority. But piecing together separate racks, cooling, power, and cable management solutions can quickly create a complex, hard-to-manage setup.   A cabinet ecosystem isn't just a single cabinet or rack; it’s an integr...
Many enterprises opt for an open architecture infrastructure as a way to drive down costs and make moves, adds and changes to equipment and cabling easy. But as newer technologies emerge, IT leaders must ensure their open architecture actually drives down costs and promot...
When it comes to organizing and setting up equipment in a computer room or data center, it is important to make the best use of the space available. For this reason, open frame server racks remain an ideal solution to help stay organized in a cost-effective manner. Rack system...
For employee owners of Chatsworth Products, Inc. (CPI), the 20 th anniversary of the company is the perfect time to look back on where we've been, where we are, and where we're going. But let's face it, the present and future are really nothing without the past, and here at ...
According to the Cisco Annual Internet Report (2018-2023), global M2M connections will grow 2.4-fold, from 6.1 billion in 2018 to 14.7 billion by 2023, and there will be 1.8 M2M connections for each member of the global population by 2023. Additionally, connected home applicat...
In today's fast-paced and rapidly evolving technological landscape, businesses must be agile, adaptive, and, above all, customer-centric. Chatsworth Products (CPI) is not just a vendor – we’re a true partner in helping to understand your specific challenges and crafting custom...
When considering the type of cable pathway that is needed to sustain and grow your network capabilities, there are several factors to consider. Things to keep in mind include, load capacity, grounding requirements, materials used, as well as the adaptability for future growth...