When managing a data center, efficiency is often a top priority. But piecing together separate racks, cooling, power, and cable management solutions can quickly create a complex, hard-to-manage setup.
A cabinet ecosystem isn't just a single cabinet or rack; it’s an integrated powerhouse where every element—from power distribution to cooling and cable management—works together seamlessly within one optimized framework.
This holistic, integrated approach boosts energy efficiency, slashes cooling costs, and provides centralized control to streamline operations. With these features already built in and scalable to your needs, your data center can evolve without incurring costly infrastructure changes.
Deploying a cabinet ecosystem requires integrating multiple elements that can be customized and preconfigured for your exact requirements. This guide walks you through six essential steps to create a customized roadmap for your ecosystem:
1. Choose a Strong Foundation with the Right Cabinet
A truly effective cabinet ecosystem begins with a strong foundation—literally. Structural integrity and cabinet strength serves as the backbone for everything else, ensuring stability, safety, and long-term durability. If you use a systems integrator to load equipment into your cabinet and then deploy, the cabinet needs to be rated to support those loads.
Ideally, your cabinet should be able to hold at least 3000 lb. (1360 kg) of equipment when attached to building structure. Reputable vendors will load-test their cabinets with a third-party laboratory using a common industry standard such as UL® 2416, the UL Standard which includes a test recommendation of up to four times their weight capacity.
The ZetaFrame® Cabinet System by Chatsworth Products (CPI) sets a new standard here, with the highest load rating on the market. Its roll-formed, tubular, and fully welded steel frame architecture supports up to 5,000 lb. in static loads and 4,000 lb. in dynamic loads, giving you the structural integrity to support your setup now and as it scales.
But strength is just the start. Right out of the box, the ZetaFrame Cabinet System offers integrated grounding and bonding, advanced cable management, and optional airflow management accessories. With high customization options in dimensions and configurations, ZetaFrame not only serves as the backbone of your cabinet ecosystem but also adapts to your unique requirements.
2. Streamline Data Center Management with Intelligent Power Solutions
Intelligent power management is a crucial element in creating a sustainable data center. In a well-designed cabinet ecosystem, these solutions enable centralized control, helping you optimize energy usage, streamline operations, and maintain vital oversight—all through a single interface.
CPI’s intelligent eConnect® PDUs are built for durability and flexibility, featuring the highest temperature rating in the market at 149°F (65°C) and configurations that can adapt to your growing power needs. Their low-profile locking outlets help prevent accidental disconnections, adding an extra layer of reliability.
By connecting eConnect PDUs with DCIM software like Power IQ® you gain real-time insights into power usage, environmental conditions, and security alerts, all from one dashboard. This holistic view allows you to make better decisions and identify areas for improvement, all while ensuring your data center is running as efficiently as possible. You can even take Power IQ for eConnect for a test drive to see how it works in practice. Plus, with Secure Array® IP Consolidation, you can manage up to 48 PDUs through one IP address, cutting down on network complexity and costs.
To simplify your setup, CPI offers pre-installation of eConnect PDUs in your ZetaFrame Cabinet. This means your cabinet ecosystem is ready for efficient performance from day one, saving you time and resources during installation.
3. Achieve Maximum Efficiency and Sustainability with Integrated Cooling Solutions
Effective cooling underpins the entire cabinet ecosystem—quietly reducing power demands, enhancing overall efficiency, and bringing sustainability goals within reach. A well-designed cabinet ecosystem optimizes cooling in two key ways.
First, proper airflow management—which is often overlooked—is essential to prevent energy waste. A cabinet ecosystem integrates advanced, built in airflow solutions, keeping hot and cold air separated so that cooling is directed exactly where it’s needed with less waste. Within the cabinet, accessories channel cold air through equipment while blocking hot air from recirculating. In the room, solutions like CPI’s Vertical Exhaust Duct (VED) isolate hot air and direct it back to air handlers, reducing bypass airflow and inefficient air mixing that can create energy losses from day one.
The second part of a robust cooling strategy is active cooling, such as liquid cooling. CPI offers a hybrid solution by integrating the ZetaFrame Cabinet System with ZutaCore's HyperCool® waterless direct-to-chip (DTC) technology. This waterless liquid cooling method delivers cooling directly to the chip in a space-saving design. This approach can improve energy efficiency by 30-50% over traditional cooling, and because it’s waterless—converting liquid to vapor upon absorbing heat—it’s safer and more cost-effective.
With a cabinet ecosystem from CPI, both airflow management accessories and liquid cooling can be preinstalled, enabling significant energy savings and supporting a more sustainable operation from day one.
4. Proactively Monitor the Environment at the Cabinet Level
One of the most common causes of downtime is hardware failure resulting from exceeded temperature or humidity levels within the cabinet. A big advantage of a cabinet ecosystem is having a clear picture of what’s happening inside your equipment at all times.
It is important to measure, and track inlet and outlet temperature and inlet humidity at each rack/cabinet to assure conditions are within ASHRAE recommended limits. A good strategy is to place a temperature and humidity probe near the top front and rear of each cabinet.
With environmental monitoring integrated into your cabinet ecosystem, you can spot and respond to issues early, adjusting as needed to avoid overcooling or overheating. This not only cuts down on energy waste but also makes sure resources are used efficiently.
CPI’s eConnect® PDUs put environmental monitoring at your fingertips, letting you remotely monitor and control temperature and humidity levels right from the cabinet. For a broader view across your entire environment, CPI’s Remote Infrastructure Management (RIM) Systems give you extended monitoring capabilities, helping you catch issues early and prevent costly downtime.
5. Secure and Protect Equipment Remotely
Physical security works best when integrated with other systems to keep things simple and efficient. By building security directly into the cabinet ecosystem, you reduce the need for extra hardware and power, creating a setup that’s easier to manage and more sustainable.
Take CPI’s RFID Electronic Lock Kit for example. Paired with eConnect PDUs, it offers an easy, all-in-one solution for managing cabinet access, power, and environmental conditions from a single interface. This setup allows you to keep a remote log of every cabinet access with an audit trail feature, so you’re always in the loop about who accessed which cabinet, and when.
What’s convenient is that the lock kit works directly with the eConnect PDU, so you don’t need to worry about separate networking or power for the locks. Everything runs through the PDU, giving you one place to manage power, monitor environmental conditions, and control access—making your security setup simpler and more sustainable.
To make installation even easier, the lock kit can come preinstalled in the ZetaFrame Cabinet, saving you time and helping you get up and running quickly.
6. Improve Airflow and Efficiency with Built-In Cable Management
In a scalable and efficient cabinet ecosystem, every detail matters, and cable management is no exception. Your cabinet ecosystem should include specific and physically separate pathways for power and network cables and mounting locations for power distribution units (PDUs) that minimize interference with airflow through the cabinet.
When cable management is built into the cabinet—like in CPI’s ZetaFrame Cabinet—it helps keep cables neatly routed and out of the way, which reduces the risk of overheating. This system makes accessing equipment and troubleshooting much easier, eliminating the hassle of untangling messy cables or dealing with cluttered external cable trays.
The ZetaFrame Cabinet features vertical cable managers that provide organization right at the rack unit level, allowing cables to be routed precisely where they’re needed. Additionally, front-to-rear style managers attached to the equipment rails help ensure smooth cable routing between the front and back, enhancing both accessibility and airflow.
As you build a scalable and efficient cabinet ecosystem, don’t underestimate the power of good cable management. It may seem like a small detail, but its impact on organization, efficiency, and ease of maintenance is substantial, making it a vital part of your overall design.
Bonus: Pre-Installation and Configuration for Fast Deployment
Time is money when setting up your cabinet ecosystem, and CPI delivers rapid solutions from a single source. Our fully integrated systems arrive pre-installed and ready-to-go, slashing deployment times while reducing packaging waste and costs.
At CPI, customization is our strength. Whether you need unique mounting brackets, modified panels, or specialized kitting, we’re here to build a solution that’s precisely right for you.
Contact our team today to discover how CPI can help you create a more efficient and sustainable cabinet ecosystem. Let’s get started on making your setup as smooth as possible!