CPI Blog

Shaping the Future of Connectivity: Key Advancements in Wi-Fi 7

January 29, 2025

The continuous evolution of Wi-Fi technologies is largely driven by the ever-increasing need for faster, more reliable, and efficient wireless communication to accommodate the growing number of devices and the more complex demands of both consumers and businesses. Ongoing advancements in Wi-Fi standards focus on addressing these challenges while supporting the progression of technology.

In part one of this blog series, we discussed the key factors driving the development of Wi-Fi 7. In this blog, we will explore the key innovations that Wi-Fi 7 brings, highlighting how these developments enhance connectivity and improve the overall wireless experience.

blog-graph-wi-fi-7-evolution-600px.jpeg

Setting the Stage: How Wi-Fi 6 and Wi-Fi 6E Pave the way for Wi-Fi 7

Before diving into the advanced features of Wi-Fi 7, it's essential to first recognize the revolutionary technological strides made by Wi-Fi 6 and Wi-Fi 6E, which serve as the crucial foundation for the innovations found in Wi-Fi 7.

Wi-Fi 6, referred to as IEEE 802.11ax, marked a significant turning point in the world of wireless connectivity. As the need for faster, more reliable connectivity increased, Wi-Fi 6 introduced several key advancements that significantly enhanced the overall performance of wireless networks.

One of its most notable features was its ability to increase speed and capacity, allowing networks to accommodate high-density environments like enterprise offices, stadiums, educational institutions, and healthcare facilities. The following are the key technological innovations of Wi-Fi 6 that reshaped connectivity.

Groundbreaking Innovations of Wi-Fi 6

  • OFDMA: Orthogonal Frequency Division Multiple Access (OFDMA) is a technique used to transmit data by splitting a signal into multiple smaller sub-signals, each delivered over a different frequency. This method helps to improve data rates and reduce interference in wireless communication. OFDMA is an advanced version of OFDM used in previous Wi-Fi iterations, where the available sub-channels are divided among multiple users or devices simultaneously. While OFDM allocates the entire spectrum to a single device, OFDMA allows multiple devices to share the same channel by assigning them specific sub-channels, improving efficiency and reducing congestion in high-traffic environments.
  • 8 x 8 MU-MIMO UL/DL: (Multi-User - Multiple Input, Multiple Output Uplink/Downlink), which was previously only available for downlink traffic in Wi-Fi 5. Wi-Fi 6 MU-MIMO supports both uplink and downlink transmission, allowing the router to simultaneously serve multiple devices in both directions. This significantly boosts network capacity and reduces wait times for each device, improving overall performance when multiple devices are connected. One of the key differences between Wi-Fi 6 and Wi-Fi 5 lies in the number of spatial streams supported. Wi-Fi 5 (802.11ac Wave 2) typically supports up to 4x4 DL MIMO, allowing it to transmit data across four spatial streams simultaneously (four transmit and four receive.) This configuration works well for environments with moderate device density but can become strained as the number of connected devices increases. In contrast, Wi-Fi 6 (802.11ax) introduces 8x8 MU-MIMO UL/DL, doubling the capacity to handle up to eight transmit and eight receive spatial streams at once both uplink and downlink. This enhancement significantly improves network throughput, especially in high-density environments with many connected devices.
  • TWT: (Target Wake Time): A key feature designed to improve energy efficiency, particularly for battery-powered devices in the Internet of Things (IoT) ecosystem. TWT allows devices to schedule specific times to wake up, transmit data, and then return to sleep mode, rather than constantly listening for transmissions. This reduces the amount of time devices need to be active on the network, conserving battery life and reducing overall power consumption. TWT is especially beneficial for devices like smart sensors, wearables, and other IoT devices that rely on extended battery life. By optimizing how and when devices communicate with the network, TWT helps to improve overall efficiency and performance, while also allowing for longer usage times between charges.
  • 1024-QAM (Quadrature Amplitude Modulation): 1024-QAM is a significant upgrade from the 256-QAM used in Wi-Fi 5. This modulation technique increases the amount of data that can be transmitted in a single signal by encoding more bits per symbol. With 1024-QAM, Wi-Fi 6 can transmit up to 10 bits of data per symbol, compared to the 8 bits per symbol with 256-QAM. The main benefit of this higher-density modulation is the ability to achieve faster speeds and more efficient use of available bandwidth, particularly in high-density environments. This results in faster download and upload speeds, making it particularly valuable for high-bandwidth and streaming applications such as 4K/8K video, online gaming, virtual reality (VR,) and augmented reality (AR.) By packing more data into each transmission, Wi-Fi 6 can provide faster, more reliable connections, further enhancing the overall user experience.

Collectively, these Wi-Fi 6 enhancements tackle challenges such as network congestion, slow speeds, and device overload in high-density environments and demanding applications. They lay the groundwork for future technological advancements in an increasingly connected and data-driven world.

The Leap to Wi-Fi 6E

blog-wifi-6-inline-350px.jpeg

Building upon the foundation of Wi-Fi 6, Wi-Fi 6E further expands its capabilities by introducing access to the 6 GHz band. The FCC’s allocation of 1200 MHz of additional unlicensed bandwidth in the 6 GHz frequency band marks a significant expansion of the available wireless spectrum.

This additional contiguous channel spectrum provides crucial benefits, helping to meet the increasing demands of Wi-Fi networks in high-traffic environments. It not only improves network performance by offering more bandwidth for faster speeds and reduced congestion but also lays the groundwork for future advancements. As wireless technologies continue to evolve, this expanded spectrum will play a key role in enabling Wi-Fi to seamlessly integrate with other technologies such as 5G, IoT, and emerging wireless innovations, driving greater connectivity and efficiency across a wide range of applications.

Traditionally, Wi-Fi has operated in the 2.4 GHz (2400 to 2495 MHz) and 5 GHz (5170 to 5835 MHz) non-contiguous channels (Figure 1 below).

blog-fcc-us-5-ghz-channel-plan-graphic-600px.png
Figure 1: FCC U.S. 5 GHz and 2.4 GHz ISM Channel Plan

Non-contiguous channels in a frequency band refer to frequency allocations that are spread out across the band with gaps between them, meaning the spectrum is fragmented. The fragmentation can also result in more complex signal processing, as devices must manage the gaps between frequency blocks, which can cause inefficiencies and reduce network performance, especially in high-density environments or when many devices are connected to the same network.

In contrast, contiguous channels are uninterrupted, with frequency blocks running continuously within the band, without gaps. The key difference between non-contiguous and contiguous channels lies in efficiency and performance. Contiguous channels allow for more efficient use of the spectrum since data can be transmitted over a broader, uninterrupted bandwidth. This leads to higher throughput, better utilization of available spectrum, and reduced latency, as the network doesn't have to jump between different frequency blocks. This is especially beneficial for high-demand applications like streaming, gaming, or large data transfers, which require stable, high-speed connections.

The introduction of the 6 GHz band (5.925 to 7.125 MHz) offers a much broader range of frequencies (See figure 2 below.)

blog-fcc-us-6-ghz-channel-plan-graphic-600px.png
Figure 2: FCC U.S. 6 GHz Channel Plan

This additional spectrum provides contiguous wider channels, up to 7 additional 160 MHz, and 14 additional 80 MHz channels, allowing for faster speeds, greater capacity, and reduced interference from other devices. With less congestion in the 6 GHz band and contiguous channels, networks can deliver improved performance, particularly in high density environments.

This is especially beneficial for high-bandwidth environments where low latency and high throughput are essential. The 6 GHz band is also less crowded compared to the lower frequency bands, enabling Wi-Fi 6E networks to maintain faster, more reliable connections, even in dense environments. As the demand for faster, more efficient wireless communication continues to grow, the 6 GHz band will play a crucial role in supporting the future of high-performance Wi-Fi.
 

Key Advances of Wi-Fi 7: Unlocking the Future of Wireless Connectivity

Wi-Fi 7, based on the IEEE 802.11be standard, referred to as Extremely High Throughput (EHT), is set to revolutionize wireless connectivity by meeting the rising demands for more efficient networks.

Building on the foundation laid by Wi-Fi 6 and Wi-Fi 6E, Wi-Fi 7 introduces several key improvements that will empower consumers, businesses, and industries to benefit from faster and more reliable wireless communication. These innovations are essential as connectivity becomes increasingly integrated and interconnected, with the demand for seamless, high-bandwidth applications growing steadily.

blog-chart-wi-fi-7-intel-600px.png

Pivotal Innovations in Wi-Fi 7:

Faster Speeds with 320 MHz Channel Width:

Wi-Fi 7 introduces 320 MHz super wide channel widths, which is double the maximum width offered by Wi-Fi 6 (160 MHz). Channel width is a key factor in determining network speed and performance. By doubling the available channel width, Wi-Fi 7 can transmit much more data simultaneously, significantly increasing throughput.

This is particularly beneficial for high-demand applications like artificial intelligence (AI), 8K video streaming, virtual reality (VR), augmented reality (AR), and cloud-based networking, gaming, which require ultra-fast and reliable connections. With 320 MHz, Wi-Fi 7 can achieve much higher aggregate link speeds, surpassing the speeds provided by its predecessors.

Enhanced Efficiency with Multi-Link Operation (MLO)

One of the standout features of Wi-Fi 7 is Multi-Link Operation (MLO). This technology enables devices to transmit and receive data across multiple frequency bands simultaneously, including 2.4 GHz, 5 GHz, and 6 GHz bands. MLO allows for faster data transfers and more reliable connections, as it can leverage the best available band in real-time, optimizing the path for data to travel.blog-multi-link-inline-200px.png

For example, if one band is experiencing congestion or interference, MLO can switch to another band, ensuring a continuous and high-quality connection. This approach improves efficiency, reduces latency, and enhances overall network performance, especially in complex environments where multiple devices are competing for bandwidth.

Increased Capacity with 4096-QAM

Wi-Fi 7 adopts 4096-QAM (Quadrature Amplitude Modulation), an upgrade from Wi-Fi 6’s 1024-QAM. QAM is a modulation technique used to encode data into radio signals, and the higher the QAM value, the more data can be transmitted per signal. By supporting 4096-QAM, Wi-Fi 7 can transmit up to 12 bits per symbol, allowing for more efficient use of the available spectrum and enabling faster data transfer rates.

This is especially beneficial in high-density environments where many devices are connected to the network simultaneously, such as stadiums, office buildings, and public venues. Higher QAM capabilities increase throughput, making Wi-Fi 7 ideal for applications that require massive amounts of data, such as ultra-high-definition video streaming, immersive gaming, and large-scale enterprise networks.

Lower Latency with Improved Scheduling

Wi-Fi 7 introduces improved scheduling techniques that enable lower latency in wireless communication. One of the key technologies contributing to this is Enhanced Scheduling through OFDMA (Orthogonal Frequency Division Multiple Access). OFDMA allows a Wi-Fi router to divide channels into smaller sub-channels and assign them to multiple devices, enabling simultaneous communication between the router and various devices.

Wi-Fi 7 enhances this by allowing even more precise control when devices access the network. This results in faster, more efficient data delivery, reducing lag and improving responsiveness, which is particularly important for real-time applications like gaming, video conferencing, and AR/VR experiences.

Improved Network Management with Target Wake Time (TWT)

Wi-Fi 7 improves upon Wi-Fi 6’s Target Wake Time (TWT), a feature that allows devices to schedule when they wake up to send and receive data, rather than continuously listening for transmissions. This feature improves energy efficiency, particularly for battery-powered devices like IoT sensors, wearables, and smart home devices.

Wi-Fi 7 optimizes this further by allowing devices to manage their wake-up schedules more efficiently, reducing power consumption and enhancing the overall efficiency of the network. This improvement is particularly valuable in environments with many IoT devices, where maintaining battery life while ensuring reliable connectivity is critical.

Wider Spectrum with the 6 GHz Band

Building on the success of Wi-Fi 6E, which introduced access to the 6 GHz band, Wi-Fi 7 continues to take advantage of this additional spectrum. The 6 GHz band offers more bandwidth, reducing interference and congestion that can be common on the 2.4 GHz and 5 GHz bands. By expanding the available spectrum and offering wider channels (up to 320 MHz), Wi-Fi 7 can support more devices simultaneously with higher performance.

This is especially useful in environments with a high device density, such as stadiums, airports, and urban areas, where network congestion can be a problem. The 6 GHz band provides faster speeds and more reliable connections, helping to meet the increasing demand for data in the modern, connected world.

Optimize Bandwidth Utilization with Multi Resource Units (RU) and Puncturing

The key difference between Wi-Fi 6/6E and Wi-Fi 7 in terms of Multi-RU and Puncturing lies in Wi-Fi 7’s enhanced ability to improve spectrum efficiency and network performance. In Wi-Fi 6, resource units (RUs) are allocated in a traditional single-unit manner, meaning that if any part of a high-speed channel is occupied by a device, the entire channel becomes unavailable, forcing the system to switch to a different channel. This limits flexibility and reduces spectrum efficiency.

Wi-Fi 7, however, introduces Multi-RU functionality, allowing a single device (STA) to simultaneously access multiple resource units. This flexibility optimizes bandwidth utilization and enhances throughput, particularly in dense environments with many connected devices.

Wi-Fi 7 also introduces Puncturing, a new feature that enables the system to bypass interference by "puncturing" parts of the channel affected by congestion or noise. This capability is absent in Wi-Fi 6/6E, which can suffer from performance degradation in crowded or noisy environments.

The Future of Wireless is Here

Wi-Fi 7 is set to be a transformative leap forward in wireless technology. By refining and enhancing the features of Wi-Fi 6/6E, Wi-Fi 7 represents a true leap forward in wireless connectivity.

With wider channel bandwidths, advanced modulation techniques, and improved handling of multiple devices on the network, Wi-Fi 7 is poised to revolutionize wireless connectivity, paving the way for a future of ultra-fast, reliable, and efficient wireless communication that delivers exceptional user experience.

 

Posted by Bree Murphy, RCDD Applications Engineer at 1/29/2025 11:07:01 AM
Search CPI in the News
Get Blog Updates
Stay up to date on latest news and solutions.