September 03, 2009
Question: We are currently calculating PUE on a monthly basis and I am looking for ways to make the information more meaningful to others in IT. What type of metrics are you using to show how PUE effects the green effort?
Answer: Power Usage Effectiveness (PUE) is useful as a benchmark for making comparisons ...
August 04, 2009
I'm an application, systems management, and middleware admin if you will, so when it comes to an actual data center from the computer decking up, I have little experience, so with that, I was not sure of how to ask the question, but I was hoping for a list of document names I should expect from someone building a data center or if I built a data center. My client is very small and this is almost pro bono (small startup city).
July 29, 2009
How important is data center thermal management energy efficiency? How about cashing in a 50 percent reduction in cooling energy on a one megawatt data center for $1.9 million savings over the life of the data center?
July 08, 2009
Question: What are your recommendations on fan controls and the best points to use for driving a feedback loop?
I have been reading quite a bit about Chatsworth for the past five months, and now we have an opportunity to install the cabinets, which is very exciting to be perfectly honest, but I wanted to run something by you.
I was thinking about the controls to implement for this project, I know from reading when there is a raised floor, the strategy can be as simple as pressure transducers ...
June 11, 2009
Question: My data center is a limited floor space (1600 sq) and running at 18 kW per cabinet. The cooling experts are indicating that a load of 18 kW would require about 2700 CFM to cool the equipment. They also indicate that max let through on a "Tate" floor tile is 1300 CFM. In this scenario we designed a wider cold aisle to accommodate a (2:1 - 2.5:1) floor tiles to enclosure ratio to meet the CFM required by the equipment.
This scenario leads to the potential of high density exceeding traditional cooling capabilities whether using CPI's Vertical Exhaust Duct or not, if there is not the floor space for additional perf tiles then your equipment cold air demand can potentially exceed the let through ratio. If true, would there be a watt per square foot - line/threshold, based on traditional cooling, raised floor height etc ...
June 01, 2009
Question: What floor tile perforation pattern (percentage open) do you recommend in data centers using cabinets with Vertical Exhaust Ducts?
Answer: If your data center uses CPI cabinets with Vertical Exhaust Ducts (VED) such at the F-Series TeraFrame Cabinet or the T-Series SteelFrame Cabinet, it ultimately does not matter where the air comes from or how it gets into the data center. However, since we have not addressed this particular subject before, your question represents an opportunity to talk further on the subject.
We recommend using one style of perforated tile through-out the space. Varying tile styles creates a mind-set for micro-managing the tile deployment, which is completely unnecessary ...
May 26, 2009
We often receive questions from folks in the industry about our products and solutions. Bill Watts, CPI Sr. Data Center Architect, responds to a customer who has three questions concerning CPI Passive Cooling®.
Question: Should I use side panels on bayed cabinets?
Answer: Although we recommend side panels on bayed cabinets you
April 14, 2009
We often receive questions from folks in the industry about our products and solutions. Bill Watts, CPI Sr. Data Center Architect, responds to one.
Question: Is there a need to "balance" the air volume with the chimney solution when racks utilize different kW? Can I use chimneys on some cabinets and allow other cabinets to function without chimneys?
February 26, 2009
Recently one of our customers, who are planning to install CPI cabinets in a new data center, was wondering if Air Dam Kits are really necessary to their overall cooling strategy. Ian Seaton, CPI Marketing Technology Manager, explains the importance
February 02, 2009
Power requirements at the cabinet level are becoming more demanding from a standpoint of equipment density of a single cabinet and the power input requirements of this equipment. In the past, one (or two, if redundancy is to be considered) single-phase power strips would satisfy most power needs. With the advent of sophisticated network switching, blade server technology, built in power supply redundancy ...