Oberon™ Skybar™ Environmental Enclosures

These outdoor Wi-Fi access point enclosures feature concealed hinges and mounting features, rounded corners, and aesthetically colored and textured surfaces.
Browse Skybar (0 Products)
Oberon™ Skybar™ Environmental Enclosures 1020 now has the NEMA PW ancillary rating indicating it has passed applicable tests for power washing. Oberon™ Skybar™ Environmental Enclosures 1020 compact NEMA 4 AP enclosure is designed specifically to protect APs in challenging environments such as stadiums, auditoriums, gymnasiums, industry and outdoors.

 

NOTE: 6 GHz Access Points (e.g. Wi-Fi 6E) may only operate outdoors in the United States in the Standard Power mode (requiring AFC coordination). Low Power Indoor (LPI) Access Points are restricted to indoor only operation.

3 options
Starting at $145.00 USD MSRP
This NEMA 4 enclosure is designed specifically to protect and conceal APs, antennas, and cabling in environments where aesthetics is paramount, and typical 'industrial' NEMA 4 enclosures are not acceptable due to their appearance.

NOTE: 6 GHz Access Points (e.g. Wi-Fi 6E) may only operate outdoors in the United States in the Standard Power mode (requiring AFC coordination). Low Power Indoor (LPI) Access Points are restricted to indoor only operation.
1 option
Starting at $280.00 USD MSRP
Oberon™ Skybar™ Environmental Enclosures 1022 has the NEMA PW ancillary rating indicating it has passed applicable tests for power washing. Oberon™ Skybar™ Environmental Enclosures 1022 is designed specifically to protect access points in challenging environments such as stadiums, auditoriums, gymnasiums, industry and outdoors. 

NOTE: 6 GHz Access Points (e.g. Wi-Fi 6E) may only operate outdoors in the United States in the Standard Power mode (requiring AFC coordination). Low Power Indoor (LPI) Access Points are restricted to indoor only operation.
1 option
Starting at $280.00 USD MSRP
This compact NEMA 4X Oberon™ Skybar™ Environmental Enclosure is designed to protect wireless LAN APs with internal or external antennas in challenging indoor/outdoor environments. This rugged polycarbonate enclosure protects the AP from weather, dust, and impacts, and is transparent to wireless signals so APs with body integrated antennas or small detachable antennas may be protected. 

NOTE: 6 GHz Access Points (e.g. Wi-Fi 6E) may only operate outdoors in the United States in the Standard Power mode (requiring AFC coordination). Low Power Indoor (LPI) Access Points are restricted to indoor only operation.
2 options
Starting at $200.00 USD MSRP
Oberon™ Skybar™ Environmental Enclosures 1026 protects access points (APs) with internal or external antennas from all vendors in challenging indoor/outdoor environments. This rugged polycarbonate enclosure protects the AP from falling water, dust, and impacts, and is transparent to wireless signals so APs with body integrated antennas or small detachable antennas may be protected. The enclosure has a hinged door, molded-in padlock hasps for locking, and interior ABS panel for attaching APs.

NOTE: 6 GHz Access Points (e.g. Wi-Fi 6E) may only operate outdoors in the United States in the Standard Power mode (requiring AFC coordination). Low Power Indoor (LPI) Access Points are restricted to indoor only operation.
14 options
Starting at $210.00 USD MSRP

Oberon™ Skybar™ Environmental Enclosure 3000 is an outdoor concealment shroud for concealing Wi-Fi and small cell APs, antennas, remote radio heads, cabling and connectors. Oberon™ Skybar™ Environmental Enclosures 3000 includes a paintable, rugged ABS plastic hinged cover which is virtually transparent to wireless signals. 
 

NOTE: 6 GHz Access Points (e.g. Wi-Fi 6E) may only operate outdoors in the United States in the Standard Power mode (requiring AFC coordination). Low Power Indoor (LPI) Access Points are restricted to indoor only operation.

1 option
Starting at $510.00 USD MSRP